Event-based Action Objects

These Action Objects (AO) are user defined calculations scheduled to execute in an event-based (triggered) fashion. They are triggered to execute by an external event, or a user’s choice to trigger them in an external application.

All triggered Event-based Action Objects will display the following information:

Header

Description

Name

The name given to the new Action Object.

The default name is the name of the blueprint or data recipe file and the AO will be deployed with this name. If a name clash occurs, names will automatically be made unique.

Status

Waiting: The Action Object is waiting to be triggered to deploy the Action Object.

Executing: The Action Object has been triggered, and is currently executing.

Total executes

The number of times the Action Object has executed.

Failed executes

The number of times the Action Object has failed to execute.

Last status

Success or failure: describes the status of the last execution.

Last event

The date and time of the last trigger event.

Last start

The start time of the last executed Action Object.

Last end

The end time of the last executed Action Object.

Total time

The duration of the execution.

Average execution time

The average duration of all the executions of that Action Object.

Source

Indicates who or what triggered the execution of the Action Object.

 

Related topics:

 

CSense 8.5- Last updated: July 10,2025